AXIS#.WS.DISTMAX
Description
This parameter sets the maximum movement that is allowed for finding commutation. If this value is too small,F5501 , "Wake and Shake - Excess movement.", may occur before wake and shake is finished. The larger this value, the more movement is allowed for wake and shake. This value is application dependent.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
deg (position units) |
|
Range |
0 to 90 deg |
|
Default Value |
15 deg |
|
Data Type |
Float |
|
See Also |
N/A |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.WS.DISTMAX | 0x5013 | 0xC | DINT | - | Position | RW | False |
| AXIS2.WS.DISTMAX | 0x5113 | 0xC | DINT | - | Position | RW | False |